Key
Starts or stops running a client key file.
Syntax
Key <
component
| /R>
where
<component>
is a relative or absolute reference to the client key file. If the file name has a space in it, enclose the name in quotes./R
stops running the client key file.Remarks
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a FactoryTalk View Studio
or HMI Server.If you run Key (component) and a file is already running, the active file is replaced by the specified file.
Provide Feedback