DisplayClientOpen

Opens the specified FactoryTalk View SE Client.
Syntax
DisplayClientOpen
<FileSpec>
where
<FileSpec>
is the name of the FactoryTalk View SE Client configuration file (.CLI) you are attempting to open. The name may include the path to the file.
Remarks
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a
FactoryTalk View Studio
or HMI Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal