DerivedOff
Stops running the specified derived tag file.
Syntax
DerivedOff <
component
>
where
<component>
is a relative or absolute reference to a Derived Tag file. If the file name has a space in it, enclose the name in double quotes.Remarks
This command can be issued from the
FactoryTalk View SE
Client, FactoryTalk View Studio
, or HMI server, but is always run on the HMI server.Provide Feedback