SetFocus
Sets the focus to a particular graphic display.
Syntax
SetFocus <
display
>
where
<display>
is a relative or absolute reference to a graphic display. If the file name has a space in it, enclose the name in quotes.Remarks
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a FactoryTalk View Studio
or HMI Server.Provide Feedback