RecipeRestore

Reads the values from a recipe file into all numeric input objects in the active graphic display. This command is used with the
Recipe
field.
Syntax
RecipeRestore <
component
>
where
<component>
is a relative or absolute reference to the recipe file that is to be saved. If the file name has a space in it, enclose the name in double quotes.
Remarks
This command is run on the currently active display on the
FactoryTalk View SE
Client or
FactoryTalk View Studio
that issued the command. It will be ignored when it is issued from an HMI Server or if no display is active.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal