PullForward

The
PullForward
command moves the specified graphic display in front of all other windows.
If the specified graphic display is of the Replace or Overlay type, PullForward gives the specified display focus and positions it behind any On Top display that is open.
Syntax
PullForward
<display>
where
<display>
is a relative or absolute reference to a graphic display. If the file name has a space in it, enclose the name in quotes.
Remarks
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a
FactoryTalk View Studio
or HMI Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal