Pin

Pins the active display on top when a
Replace
display opens at runtime.
Remarks
This command applies to the
On Top
display only.
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a
FactoryTalk View Studio
or HMI Server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal