Examples: Display command

Display Sample /X100 /Y150
This positions the graphic Sample 100 pixels from the left edge of the screen and 150 pixels from the top of the screen. If the graphic does not fit entirely inside the FactoryTalk View SE Client window, it is truncated and scroll bars are displayed.
Display Picture /Pnames /CB
Positions the graphic display Picture in the center of the bottom half of the screen, using the parameter file
Names
, to replace tag placeholders with tag names.
Display picture /h300 /w400 /CC
Makes the graphic display Picture 300 x 400 pixels and positions it in the center of the screen.
Display /area1::Picture
Shows the graphic display Picture from area1.
Display PIDE /CC /M4
When executing the command on the fourth monitor, the graphic display PIDE is shown in the center of the screen of the fourth monitor.
Display PIDE /CC
Without the /M parameter, the graphic display PIDE is shown in the center of the current monitor on which the
Display
command is executed.
Display PIDE /H${Tag1}$ /W${Tag2}$
Shows the graphic display PIDE, while placeholder Tag1 is substituted with its tag value as the height and Tag2 is substitute with its tag value as the width.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal