DisplayNextScreen
Opens the next graphic display in the navigation history.
This command is run only on the
FactoryTalk View SE
Client that issued it. It is ignored when it is issued from a FactoryTalk View Studio
or HMI Server.Provide Feedback