DataLogRenameFile
Changes the log file identifier string that is used as part of the file name for file sets and ODBC backup files. The change affects the current logging session only, including the current set of log files.
Syntax
DataLogRenameFile <
component
> <
LogFileIDString
>
where
<component>
is a relative or absolute reference to a data log model. If the model name has a space in it, enclose the name in quotes; for example, "Recipe Log".<LogFileIDString>
is the log file identifier string, up to 20 characters.Remarks
This command can be issued from the
FactoryTalk View SE
Client, FactoryTalk View Studio
, or HMI server, but is always run on the HMI server.Provide Feedback