DataLogChangeRate

Changes the periodic log rate. The change affects the current logging session only.
Syntax
DataLogChangeRate <
component
> <
value
> [
units
]
where
<component>
is a relative or absolute reference to the data log model. If the model name has a space in it, enclose the name in quotes, for example, "Recipe Log".
<value>
is the numeric portion of the time interval for the log rate. The value must be an integer in the range of 1 to 64,000.
[units]
is the time unit of the log rate: hundredths, tenths, seconds, minutes, hours or days. The default is seconds if you omit the [unit] parameter.
Remarks
This command can be issued from the
FactoryTalk View SE
Client,
FactoryTalk View Studio
, or HMI server, but is always run on the HMI server.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal