Example: Operator precedence
For these examples, tag_1 = 5, tag_2 = 7 and tag_3 =10.
(tag_1 > tag_2) AND (tag_1 < tag_3)
is evaluated in this sequence:1 tag_1 > tag_2 = 0
2 tag_1 < tag_3 = 1
3 0 AND 1 = 0
The expression evaluates to 0.
tag_1>tag_2 AND tag_3
is evaluated in this sequence:1 tag_2 AND tag_3 = 1
2 tag_1 > 1 = 1
The expression evaluates to 1.
NOTtag_1 AND tag_2 > tag_3 ** 2
is evaluated in this sequence:1 NOT tag_1 = 0
2 0 AND tag_2 = 0
3 tag_3 ** 2 = 100
4 0 > 100 = 0
The expression evaluates to 0.
Provide Feedback