Example: Incomplete time parameter
The following are valid examples of incomplete time parameters:
- "17:00"means once a day at 5:00 p.m.
- " :30 "means once an hour, on the half hour
- " fri 17:"means 5:00 p.m. each Friday
Provide Feedback