Add a comment to an expression

Use an exclamation mark (!) at the beginning of a new line or immediately after a semicolon (;) to add a comment. Everything between the exclamation mark and the end of the line, or the next semicolon, is treated as a comment and is not evaluated.
To add a comment:
  • In the expression, enter an exclamation mark (!) followed by an comment.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal