Copy and paste animation
You can copy the animation defined for one graphic object in a display and then paste it onto another object. Use
Copy Animation
and Paste Animation
options on the Edit
menu to do this.
TIP:
You can select the object, then open the relevant
Animation
dialog box to review the details of the animation before you copy it. You do not have to close the Animation dialog box to copy the animation, simply choose Copy Animation from the Edit menu.If the object from which you are copying animation has more than one type of animation set up, all animation is copied.
When you paste animation onto an object, it coexists with any existing animation.
To copy the animation from an object:
- In a display, click the object whose animation is to be copied, to select it.
- SelectEdit>Copy Animation. You can also right-click the object and selectCopy Animation.
To paste the animation to another object:
- Click the object to which the animation is to be copied, to select it.
- SelectEdit>Paste Animation.You can also right-click the object and selectPaste Animation.
Provide Feedback