Remove an image from an HMI project
You can remove an image from an HMI project.
To remove an image from an HMI project:
Do one of these:
- In theImagesfolder, right-click the image's name and clickRemoveorDelete.Removedeletes the file from the project but not from the disk;Deletedeletes the file from the project and the disk.
- In theImage Browser, in theSelect imagelist, select the image to be removed and then clickDelete. At the prompt, clickOKto confirm.
Provide Feedback