Use Variable Properties dialog box

Use the dialog box to configure a tag or parameter whose value is used to determine the confirmation types.
The following table shows options in the tab.
Option
Description
Tag
Enter a tag or parameter whose value is used to determine the confirmation types.
Tag value
Enter integer values for each confirmation type. No confirmation is required for the other values.
The confirmation types include:
  • Confirmation
    : requires confirmation without signature.
  • 1 E-Signature
    : requires performer's signature.
  • 2 E-Signature
    : requires performer and approver's signature.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal