Insert a numeric variable

Use the
Numeric Variable
dialog box to create a numeric variable for a text field. The numeric variable can be a tag name or placeholder that will provide a value that can change dynamically at runtime, or a literal number that will be displayed the way it is entered in this dialog box.
To insert a numeric variable:
  1. Below the text field where you want to insert the variable, click
    Insert Variable
    .
  2. Click
    Numeric
    .
  3. In the
    Numeric Variable
    dialog box, specify the options.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal