Example: Use a piloted control list selector

  1. Create a piloted control list selector with ten states. Adjust the size of the object so that it displays five states.
  2. Set the Access on the States tab to different values for the different states - Operator and Remote for some, Operator only for some, Remote only for some, and None for some.
  3. In the Communications tab, set the Value connection, the Indicator connection and the Remote Access connection to analog tags.
  4. Set either the Visible States connection or the Top Position connection to an analog tag.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal