Interlocked Push Button Properties - General tab

The following table shows options under
Appearance
of the
General
tab.
Options
Description
Border style
Select the border style. The default style is Line.
If the object is a rounded rectangle, circle, or ellipse, the available border styles are None and Line.
Border width
Type the number of pixels for the width of the object’s border.
Back style
Select whether the object background is solid, gradient, or transparent. If you select Transparent, the object’s background is not filled in and any objects behind it show through. If you select Gradient, the object's background is filled with a linear gradient color.
Specify the color for the background (Back color) in the States tab.
Shape
Select the shape of the object. If the object is a rounded rectangle, circle, or ellipse, the application applies properties such as size and position by measuring in relation to the object’s bounding box.
Tip
: Press
Ctrl
while dragging a corner of the shape to form a square button.
Corner radius
Available only when the shape is rounded rectangle. Specify how rounded you want the corners to be.
Border uses back color
Select this check box to use the object’s background color for the border of the button. If this is not checked, you can assign a separate color to the border, instead of using the object’s background color.
Specify the background color and the border color in the States tab.
Highlight color
This field displays the current highlight color. Click it to select another color.
For button objects, the button’s border, if any, changes to the highlight color when the operator presses the button at runtime.
The following table shows options under
Button Value
of the
General
tab.
Options
Description
Button Value
Type the integer value to use for this button. When the operator presses the button, the button changes to State 1 and the application sends this value to the data source.
The following table shows options under
Button Value
of the
General
tab.
Options
Description
Touch margins
You can specify a touch-insensitive margin inside the button’s edges. If the operator presses on the touch-insensitive margin, the button press is not registered.
Horizontal margin
Type the number of pixels for the horizontal touch margin. The horizontal margin is along the button’s left and right edges.
Vertical margin
Type the number of pixels for the vertical touch margin. The vertical margin is along the button’s top and bottom edges.
The following table shows options under
Other
of the
General
tab.
Options
Description
Audio
Select this check box to sound an internal beeper when the object is pressed. If the computer running the project does not have an internal beeper, the object press does not trigger a beep.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal