Numeric Input Properties - Connections tab
The following table shows the options of the
Connections
tab of Numeric Input
Properties.Options | Description |
---|---|
Value | Specify a tag that will provide a value for the numeric input object. This is a read/write connection. |
Minimum | Specify a tag, expression, or a numeric value that will define the minimum value that can be written to the numeric object. This is a read connection. |
Maximum | Specify a tag, expression, or a numeric value that will define the maximum value that can be written to the numeric object. This is a read connection. |
Provide Feedback