Configure general properties of a multistate push button
After you set up the options in the
General
tab, click the States
tab to specify how the button looks in each state at runtime.To configure general properties of a multistate push button:
- In theMultistate Push Button Propertiesdialog box, in theGeneraltab, specify the following properties if needed:
- general appearance
- number of states
- how the button changes states
- touch margins
- audio (whether the button beeps at runtime)
Provide Feedback