Causes of latched push button runtime errors

At runtime the application logs errors about the latched push button to FactoryTalk Diagnostics under these circumstances:
Invalid values
  • If the button’s state value is too large for the data type of the tag assigned to the Value connection, or if the value is outside the assigned tag’s minimum and maximum values, the application does not write the value to the Value tag, the state does not change, and the application logs an error.
    For example, the state value is too large for the tag’s data type if the data source is a PLC-5, the state value is 2,147,483,647, and the assigned tag is an integer tag using the address N7:0.
    The digital tag works like a Boolean in that any non-zero value is treated as 1.
  • If the Indicator tag value does not match any of the state values for the push button, the button displays the error state.
    The digital tag works like a Boolean in that any non-zero value is treated as 1.
Unassigned controls
  • If the Value connection is not assigned, when an operator presses the button it does not latch and the application logs an error.
  • If the Handshake connection is not assigned, when an operator presses the button it does not latch and the application logs an error.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal