Install the certificate on the associated computers
To establish encrypted connections to the database, after assigning a certificate to the SQL Server computer, set up the associated computers to trust the certificate's root authority:
- Alarms and events server
- HMI server
To install the certificate on the associated computers
- Add the snap-in.
- On theStartmenu, selectRun, enterMMCin theOpenbox, and then selectOK.
- In the Microsoft Management Console, selectFile > Add/Remove Snap-in.
- In theAdd or Remove Snap-insdialog box, selectCertificates, and then selectAdd.
- In theCertificates snap-indialog box, selectComputer account, and then selectNext.
- In theSelect Computerdialog box, keep the defaultLocal computerselection, and then selectFinish.
- In theAdd or Remove Snap-insdialog box, selectOK.
- Import the certificate.
- In the Microsoft Management Console, expandCertificates > Trusted Root Certification Authorities, right-clickCertificates, and then selectAll Tasks > Import.
- In the Certificate Import Wizard, specify the certificate file's full path, and then selectNext.
- Enter the password, and then selectNext.
- Specify the certificate store asTrusted Root Certification Authorities, and then selectNext.
- SelectFinish.
Provide Feedback