EChartsWidget
EChartsWidget is a .NET control that provides the capabilities of Apache ECharts. Apache ECharts is an open source JavaScript visualization library with a wide range of charts and graphs. Use the .NET Control object to add built-in or custom ECharts widgets on the display. The built-in widgets are pre-configured with sample JavaScript for the control's appearance and data connection, while the custom widgets provide more flexibility that you can configure with JavaScript for your own purposes.
Like any other .NET controls, a widget includes properties, methods, and events, and its actual functions are contained within its own configuration. Two specific properties of its configuration that need your attention are LanguageID and RefreshTime.
- LanguageIDSet the widget's string language with a language identifier (for example, de-DE for German) in the script. You can also use this property to switch languages.
- RefreshTimeSet the time in milliseconds that the widget refreshes its bound tag value.
For more information on ECharts, see Apache ECharts.
Provide Feedback