Deploy .NET controls on multiple computers
- For custom .NET controls, copy all the binaries in C:\Users\Public\Documents\RSView Enterprise\DotNetControl Setup on theFactoryTalk View Studiocomputer to the same folder on all client computers.
- For third-party libraries installed in the Global Assembly Cache, install them on all client computers, and then copy all the binaries in C:\Users\Public\Documents\RSView Enterprise\DotNetControl Setup on theFactoryTalk View Studiocomputer to the same folder on all client computers.
Provide Feedback