Screen Statistics dialog box
The
Screen Statistics
dialog box shows the following statistics information of the current display.- Total tags referencedThis includes all tags referenced in expressions, commands and embedded variables of the current display.Duplicated references of the same tag in an expression are counted as one tag.Each global object parameter used in an object is counted as one tag.
- Unique tags referencedThis includes all unique tags used in expressions, commands and embedded variables of the current display.
- Number of Expressions used
- Number of Alarm functions usedThis includes all FactoryTalk alarm and event functions.
- Number of Global Objects referenced
- Number of ActiveX Controls used
- Number of Security functions usedThis includes all references to the security functionsCurrentUserHasGroupandCurrentComputerHasGroup.
- Number of referenced imagesThis includes all references to images that are listed under the Images folder of theFactoryTalk ViewExplorer window.
- Number of imported imagesThis includes all references to imported bitmap or icon files for the button appearance.
Provide Feedback