Add Application Libraries to a new HMI server
You can add one or multiple Application Libraries when creating an HMI server.
To add the Application Libraries when creating an HMI server
- In theSelect Operationwindow of the Add HMI Server Wizard, click theAdd Application Librarydropdown list, and then select one or multiple libraries.TIP: The list only shows a maximum of 20 libraries.
- ClickNextand follow the on-screen instructions.
Provide Feedback