Add Application Libraries to an existing HMI server
You can add the Application Libraries after an HMI server is created.
To add the Application Libraries after an HMI server is created
- In theExplorerwindow of FactoryTalk View Studio, right-click the HMI server icon.
- Point toAdd Application Library, and then select a library to add.TIP: The list only shows a maximum of 20 libraries.
Provide Feedback