Required security settings

The following FactoryTalk security policy permission is required to run this tool:
System\Policies\Product Policies\FactoryTalk View SE\Feature Security\Category\Configure FTView SE Website
To open the
Configure Securable Action
dialog box where you can add or remove access to users and groups, double-click the
Feature Security
heading and click the browse button (...) to the right of the
Configure Security
setting.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal