WordWrap, CaptionWordWrap or St_CaptionWordWrap
Specifies whether the caption or message continues onto the next line at the beginning of a new word.
If WordWrap is False, the caption or message continues on the next line whenever the maximum text length is reached, even if this occurs in the middle of a word or number. The maximum text length depends on the Width and Font properties.
Provide Feedback