Visible or (GroupVisible)

Specifies whether to make the object or group visible.
If this is False, the object is invisible at runtime. (It is visible in the development system.)
If you are using visibility animation, the visibility animation setting overrides this option.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal