UseVariableRamp
Choose whether or not the object's Ramp value will use a tag or expression value, or a constant value, at runtime. If a constant value is used, the RampValue property must be specified. If a tag or expression value is used, the Ramp connection must be assigned.
Provide Feedback