Touch
Specifies whether or not the object is activated by touch . If you select True, the operator can press the object using a touch screen or mouse.
If you select False, the operator must use a keypad or external keyboard to press the object. In this case, use the Key Assignments editor to assign a function key to the object.
If the object’s Shape property is Circle or Ellipse, the touch area is the object’s Bounding box.
Provide Feedback