State (released and selected)

You can select a state from the list beside the State property and then set values for the ST_ properties for that particular state.
The released state is State 0. The selected state is State 1.
When the button’s control tag value equals the value for this button, the button is in State 1. If the control tag is any other value, the button is in State 0.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal