ReleaseButton method

Causes the button object to behave as if the primary mouse button is released on the button object. When an ME display is migrated to an SE display, ME Key Assignments are automatically converted to SE Display Key definitions using this method with the Invoke command.
TIP:
You will have to define another Display Key that uses the Invoke command to call the PressButton method prior calling this method.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal