ParameterList or St_ParameterList
Specifies the parameter list to run with a particular display when it is selected in the Display List Selector object at runtime.
Click the browse button
(...)
to open the Tag Browser and add tags to the parameter list. Each new tag is separated from the previous tag by a comma.A parameter list assigns tags to tag placeholders in the display when the display is opened at runtime.
Provide Feedback