ParameterFile or St_ParameterFile

Specifies the parameter file to run with a particular display when it is selected in the Display List Selector object at runtime.
Click the browse button
(...)
to open the file selector. The selector's list contains all of the parameter files associated the HMI project.
A parameter file assigns tags to tag placeholders in the display when the display is opened at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal