MaximumValue for the Value connection
Specifies the maximum value to send to the Value connection. If the DecimalPoint property is Fixed position, the maximum applies to the stripped value, not the displayed value.
If you assign a connection to the Optional Expression, the maximum also applies to the value sent to the expression.
Provide Feedback