Maximum (numeric input object)

Specifies the maximum value that can be written to the numeric input object.
Maximum can be a tag, expression, or a numeric value. At runtime, values that are downloaded by the operator are validated against the range specified by the Minimum and Maximum properties.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal