Search
FactoryTalk View SE Help
LimitValue
If the RampType property is Ramp up, specifies the amount the button’s value cannot exceed.
If the RampType property is Ramp down, specifies the amount the button’s value cannot go below.
Graphic object attributes
Provide Feedback
Have questions or feedback about this documentation? Please
submit your feedback here
.
Normal