ImageAlignment or St_ImageAlignment
Specifies how the image is positioned on the object.
If the object’s Shape property is Circle or Ellipse, the position is relative to the object’s Bounding box.
Provide Feedback