EnterKeyControlDelay
Specifies the length of time to delay between when the operator presses the Enter button and the application sets the Enter connection to 1. Assign the Enter connection in the Connections tab.
Provide Feedback