DecimalPoint

Specifies the type of decimal point to use:
  • Implicit
    - if the operator manually enters the decimal point and you want the decimal point to be used when the value is sent to the Value control.
  • Fixed position
    - if the values that are entered in the numeric pop-up scratch pad or keypad always have the same number of digits after the decimal point. If you select this type of decimal point, specify a value for the DigitsAfterDecimalPoint property. The decimal point is stripped when the value is sent to the Value control.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal