CaptionTruncate

Specifies whether or not to cut off captions that exceed the maximum length at the beginning of a new word.
If you select Character, the caption is cut off whenever the maximum caption length is reached, even if this occurs in the middle of a word. If you select Word, the caption is cut off at the end of a word. The maximum caption length depends on the width of the object and the font size.
When a caption has been truncated, the application places an asterisk at the right end of the caption to indicate that text is missing.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal