How do I view operations log

You can export a list with the operations being carried out in both the
FactoryTalk Remote Access Manager
and the
Interactive Access
Tool.
NOTE: See Log and (Interactive Access) Log for further information on these subjects.

FTRA Manager

Access
FactoryTalk Remote Access Manager
and select the
Log
section.

Interactive Access
log

  1. Access
    FactoryTalk Remote Access Manager
    and select the
    Domain view
    section.
  2. Click on the
    Interactive access
    (
    Tools
    or
    Web Only
    ) button at the top right of the screen.
  3. Select the
    Log
    section.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal