Connection between
FactoryTalk Remote Access Manager
and remote devices

The connection logic between the
FactoryTalk Remote Access Manager
and a remote device occurs as described below:
  • The
    FactoryTalk Remote Access Manager
    connects to the Server Infrastructure and obtains a list of the devices registered to the user's domain.
    NOTE: See FactoryTalk Remote Access Manager overview and related entities for further information on domains.
    NOTE: The user owns the access permissions for the aforementioned devices. See Domain user permissions for further information on this subject.
  • When you connect the remote device to the Server Infrastructure, the
    FactoryTalk Remote Access Manager
    receives a notification about this connection.
    NOTE: See (Interactive Access) Connection for further information on this topic.
  • You can establish a VPN connection trough
    FactoryTalk Remote Access Manager
    and access the
    Remote desktop
    service.
    NOTE: See (Interactive Access) Remote Desktop for further information on this topic.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal