Domain and Runtime licenses
Domain Licenses
A domain license allows the use of connection services through the UBIQUITY Manager, and it is based on the number of concurrent connections.
NOTE:
See updated details on the available domain licenses and their related features at the https://www.asem.it/en/products/14/ubiquity.html web page, under the
UBIQUITY X - Connectivity services
section.Runtime Licenses
Runtime is available in two different license types: Basic and Pro.
NOTE:
See updated details on the available Runtime licenses and their related features at the https://www.asem.it/en/products/14/ubiquity.html web page, under the
UBIQUITY Runtime - Features
section.Provide Feedback