(Interactive Access) Processes

This section shows a list including all the ongoing processes. They can be stopped by clicking the
End Processes
button.
FactoryTalk Remote Access Manager
provides a
Processes Manager
to assist in identifying running processes on remote devices, CPU usage percentage and memory usage.
To access
Processes Manager
, proceed as follows:
  1. Make sure that the
    FactoryTalk Remote Access Manager
    is connected to the remote device.
  2. Access
    Explorer
    Domain view
    VPN
    Processes
    .
    Or
    Explorer
    Domain view
    Interactive Access (Tools)
    Processes
    .
    NOTE: The
    Processes
    feature cannot be accessed through
    Interactive Access (Web only)
    .
  3. The
    End processes
    button activates.
    NOTE: Use the
    End processes
    button to end any process, as needed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal