Deployment troubleshooting
Troubleshoot issues with policy model deployment to resolve deployment errors and warnings.
General troubleshooting
- Update software, and check software compatibility. For more information, see Install or update software and the release notes.
- Check error and warning messages for possible solutions
- Check the network
- Check the physical connection of the device
- Cycle power to the device
- Retry policy model deployment
- Reset the device to factory settings
- Update device firmware
1756-EN4TR troubleshooting
1756-EN4TR devices do not support CIP Security in redundant adapter
mode.
If a 1756-EN4TR device is installed, uses CIP Security, and is reconfigured
to be part of a redundant adapter pair, the module loses its CIP Security
configuration, and the I/O chassis loses communication with the controller. To resolve the
issue, deploy the CIP Security policy again.
OPC UA troubleshooting
If CompactLogix or ControlLogix controllers are in the RUN mode, you must
power cycle the controllers to complete their configuration even if OPC UA policy
deployments succeed.
For more information about the supported CompactLogix and ControlLogix, see
OPC UA security policy.
Provide Feedback